• RE: questions about AD8351 output common voltage adjustment

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8351: single-ended-to-differential operation gain calculation

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • What is absolute max for inputs of the AD8351?

    Absolute max for inputs is not specified in datasheet

  • AD8351 Phase and Group Delay at high frequency

    Hi all,

    In the datasheet @ AD8351 rev.D,

    TYPICAL PERFORMANCE CHARACTERISTICS

    Figure 24. Phase and Group Delay (AV = 10 dB, at 5 V Supplies)

    This data is measuring between 0 to 250MHz.

    Do you have the data to provide available @ 1GHz ~2GHz?

    Best…

  • Suitable Driver for AD9681 ADC, ADL5566 or AD8351 or else?

    Dear engineers!

    I am looking for a suitable driver for the AD9681 8-channel 14bit ADC. Currently we are working with the ADL5566 and an ADC of a different vendor. We would like to replace our current ADC with the AD9681 due to its lower power consumption…

  • AD8351 suffix

    Hi

    I would like to make sure about ordering number.

    What is the difference between AD8351ARM and AD8351ARMZ ?

    I think ARMZ is just Pb free, correct?

    Regards

    moto

  • AD8351 gain calculating

    Hello ADI

    This gain formula doesn't match. Can you show me a true formula? 

    Thank you

  • AD8351在使用脉冲放大过程中,有时候出现输出叠加低配的干扰信号,此时测试共模输出引脚,发现不为1.65V(3.3V供电)?芯片可能并么有坏。

    AD8351在使用脉冲放大过程中,有时候出现输出叠加低配的干扰信号,此时测试共模输出引脚,发现不为1.65V(3.3V供电)?芯片可能并么有坏。

  • AD8351 input matching

    Hello all,

    I am trying to match the input of the AD8351 to a 100R differential source.

    In the datasheet of the AD8351 im referred to the datasheet of the AD8350 which gives me the calculations.

    Calculating with 300MHz, a Rload of 5K and a Rsource of…

  • AD8351 PWUP

    With the Vpos @5V and the Vocm set at 2.5V.  Is there any information about how fast the AD8351 will activate once the PWUP pin is above 1.3V threshold.  Also is there any data on how much current the part will draw in when PWUP is below this threshold…