• FAQ: Can AD8346 be operated at frequencies below 800 MHz?

    Question: FAQ: Can AD8346 be operated at frequencies below 800 MHz?

    Answer: For starters, there is only one good reason to try and use the AD8346 at frequencies below its specified 800 MHz minimum. And that reason is the fact that the device has…

  • ad8346最大工作结温

    ad8346汽车级最高工作环境温度是125度,最高结温是多少摄氏度?

  • RE: IQ Modulator HMC495 or AD8346

    The HMC495 is obsolete. Please use the parametric search to find a product suitable for your application:

    https://www.analog.com/en/products/rf-microwave/iq-modulators-demodulators/iq-modulators.html

  • IQ Modulator AD8346 Baseband Signal Waveform.

    Hi All,

    Can somebody send me the screenshot or plot of the Baseband input Signal for AD8346 ?

    I wish to make sure what I have understood from the Datasheet is correct.

  • AD8346的输入电压范围

    贵公司AD8346器件手册上写到“Wide dynamic input range 100 μV rms to 3 V rms (8.5 V p-p) full-scale input range Larger inputs with external scaling”,上面注明改变器件外围配置可以提高输入电压的范围,是否可以将器件配置如贵公司官网“http://www.analog.com/cn/technical-articles/simple-circuit…

  • RE: AD8346

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8346 θJC

    Hi all,

    θJC @ AD8346 is available ?

    And Maximum Junction Temperature ?

    (θJA : 125°C/W @ Absolute Maximum Ratings)

    Best regards,

    sss

  • AD8346输入交流信号隔离的问题

    使用类似AD8346的RMS to DC芯片检测交流信号电压有效值芯片,若被测信号接大地,是否需要对被测信号做隔离,若需要的话,怎样做才合适呢,谢谢!

  • AD9761 + AD8346

    Hello,

    My design is about a SAR system and I want to control the output of the I&Q Modulator (AD8346) using the AD9761. I have done the same schematic as the figure 28 of the AD8346's datasheet and the idea is to control the DAC's with an Arduino Micro…

  • AD8346使用疑问

    1、调制器

    1)AD8346是否可以用作UQPSK调制,如何实现UQPSK调制?是否可以通过改变基带信号的幅度来实现I、Q的幅度比?

    2)是否可用作BPSK调制,即只使用I路或Q路,如果只使用一路时,另外一路输入该如何处理?

    3)基带信号直流耦合还是交流耦合好?

    4)调制基带信号频率为多少较好?基带调制信号直接是0频?还是低中频、高中频?

    2、手册里讲:基带幅度为0.7V~1.7V,偏置电压为1.2V

    1)请问是需要严格满足0.7V~1.7V,还是电平在此范围内即可?

    2)偏置电压是否必须严格1…