• RE: ADL5801   Up Convertion mode with DC-50 MHz RF input

    Hi Alexius,

    My apologies, many of the "RF types" were at the International Microwave Symposium last week in Montreal so we're a bit behind in answering questions.

    To get the frequency response you want (DC-50 MHz input) you need to use…

  • RE: 求推荐一款混频器,要求幅频响应在dc--100M是线性的

    您好!

    满足您频段要求的产品请见附件内表格。

  • RE: 混频器问题

    您好!

    ADI具有集成本振的混频器芯片,为ADRF66XX系列产品。但是没有这么低频段的集成本振的混频器产品。满足您频段的混频器请见附件内表格。

  • RE: Bandwidth/Demodulation Bandwidth

    If your desired signal is at 300 MHz and you want to see phase changes, you need some sort of a phase detector, which also means you need a reference signal of constant phase. Here are some ideas, but the devil is in the details...

    1. AD8302 -- drive…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • Magnetic Compatible LNA

    Hello,

    I am working on the RF receiving coil of MRI scanner, and a magnetic compatible low noise amplifier is required to work as pre-amplifier inside the magnetic body. The magnetic field could be 1.5T or maybe up to 7T. I noticed that ADI has a document…

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF