• 关于AD8343的S参数仿真

    各位大师你们好,我现在对AD8343进行仿真,官网给的是一个S2p(二端口)的S参数文件,但是AD8343是一个3端口的混频器件,现在不知道如何进行仿真,还有在进行仿真时那个外围电路怎样设计?求懂得给一帮助!

  • RE: Recommended down convert mixer for low RF frequency input, from RF 400kHz~100MHz to IF 100kHz ?

    Hi,

    They could try AD8343. We didn't measure the part down to that frequency but it possibly could work.

    Thanks.

  • Phase detection using passive or active mixer

    Dear community,

    I wish to make a phase detection of two sinus signals. I am a beginner in the field and seeking for some advices.

    My setup would be the following:

    - DDS (i think of using the AD5932) to deliver my reference signal. I want to have a frequency…

  • AD8351 S-parameters

    Hello, I'm trying to find S-parameters for the AD8351. There is an old post on this topic (see https://ez.analog.com/rf/f/q-a/76076/question-re-ad8343-s-parameter-data/234351#234351) which states "My apologies for the long wait on the S-parameter…

  • VHF mixer and oscillator

    Hello,

    I will be design receiver with mixer with frequency range 73-84MHz and IF frequency 45MHz. I looked your mixers ( for example ADL5350, ADL5801, LTC5510, AD8342, LT5512, AD8343, LT5526) and all your mixers don ´t have any divider fo LO path. Do…

  • AD 8343 issues

    Dear Analog Devices Community,

    I
    have sampled some of your AD8343 high IP3 active mixers and want to integrate
    one of them now in my circuit design as a multiplier. For impedance matching
    you provide a S-parameter file, but I cannot figure out at which…

  • RE: 1-30MHz upconverting mixer

    Hi, Bernard,

    Regarding the AD8343, I meant to say that

        "The inputs have a low differential impedance of 5.6 ohms"

    Benjamin

  • RE: HMC915 Replacement

    Hello,

    The closest alternative is the AD8342 and AD8343 but they have different footprints.  It appears Arrow Electronics still has some HMC915LP4E in stock.

    Regards,

    Mark

  • Analog PLL for fixed frequency PLO

    Hello,

    I would like to implement an analog PLL for a fixed frequency phase-locked oscillator. RF/LO frequencies could be as low as 1 MHz or even on the hundred KHz range. Can anyone suggest a suitable doubly-balanced mixer?

    I found AD831 and AD8343…

  • Direct downconversion from 125MHz?

    Hello, for my application I need to downconvert a 125MHz carrier to quadrature baseband signals (and I really would rather it be analog, please don't roll your eyes and tell me to throw down an FPGA), and I was hoping I'd find an active mixer IC which…