• RE: AD8342

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8342 question

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8342 input matching

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • mixer AD8342 in Baseband

    Hi I would like to use this mixer ( AD8342) to use th IF port with a baseband signal with a bit rate of 9600 bauds

    Is it possible to do this. because I used the evaluation board, applying th IF port adaptation as in Figure 59 (Low frequency application…

  • RE: AD8342 - insufficient Input-P1dB ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8342 LO  Input Impedance @ PWDN

    Hi all,

    The AD8342 LO Input Impedance @ PWDN mode is Hi-z or 50 ohm?
    and LO Input min Level ,range ?

    Best regards,
    sss

  • RE: AD8342 maximum single ended input?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8342 s-parameters?

    Hello I will use this mixer, is there a s-param file to simulate?

    thanks

  • The function of AD8342-EVALZ-ND

    Dear Sir/Madam,

    I just bought the AD8342-EVALZ-ND and I read the data sheet of AD8342 which said that it could be used as both down-converter and up-converter. I want to make sure that if AD8342-EVALZ-ND can also be used as both a down-converter and an…

  • RE: Use AD8342 for Tx and Rx path

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,