Hi
We are planning to implement AD834 multiplier in our board. Is there any evaluation board for this part?
Regards
Srikanth Kacchu
Hello,
Figure 23. Wideband Three-Signal Multiplier/Divider is incorrect in Rev. F of the datasheet: The Y2 input of the lower ad834 is incorrectly left floating.
Hello
I want to use analog multiplier to multiply the two amplitudes and output the products, which is its theory of operation. unfortunately I do not see it working the way it should. I do not see any variation of output with the change in input amplitudes…
I am trying to build mean square circuit using multiplier AD834. I am using circuit diagram provided in Analog devices application note AN-212. In fig.3 on page 6-41 of this application note there is simple DC to 500MHz Mean Square circuit. When I input…
When tested at a temperature below 0 C, the signal dropped sharply to -30...-50 mV(0.7 mV under normal conditions). Removed the capacitors standing in the integrator. Soldered the feeder through the capacitance and resistance to the output. Detected oscillation…
我想设计一个(20到200MHz)乘以100HZ的乘法器电路,能否用AD834?主要的目的是要想实现一个双边带的调制信号。就是输出只有(20到200M)加100HZ 和(20到200M) -100HZ,用AD834能行吗?ADL5391和834除了频范围上的差别还有其他吗?ADL5391也是4象限乘法器吗?
On the Data Sheets I found the "Full-Scale Range" (+- 1V) and the "Clipping Level" (+- 1.3V), but nothing about the input common mode voltage (with +-5V power supplies).
调制方式
幅度调制
调制信号(外部输入)
90Hz、150Hz、1020Hz单信号及合成信号
调制度
可调,最大深度为40%±2%
调制度差精度
90Hz和150Hz的调制度差稳定性优于±0.5%
我想用ADI的乘法器来做,比如AD834…
Dear all
My circuit design is followed analog devices suggestion(see as attachment 1 Fig.13)
And It said its bandwidth is about 480MHz.
What I need is a analog multiplier which transfer function W-output=Input1(t)*Input2(t).
And the bandwidth over…
我按着手册上的图(图一)做了一个电路图,原理图是如图二,巴伦用的是TC1-1-13的型号,出现了个问题。
1、X,Y的输入都是1V的正弦波信号,输入频率也是一样的,相当于倍频把,但是当我输入频率增加的时候,-3dB带宽连100MHz都达不到,是我电路的问题吗?
2、手册上写的带宽能到500MHz才对,还是说500MHz的不是用图一的电路图,应该用图三?这两个图有什么区别吗?区别是什么?变压器带抽头和不带抽头有差吗?CT端接电源又是为什么呢?如果用图三的电路应该选择什么型号的变压器可以呢?