• RE: Ultrasound Transducer Integrated Pre-amp

    Thank you for answering.

    I don't know about the circuit, but the PCB on the right photo seems to combine your recommended devices.

    I wonder if you can customize the PCB to meet our requirements like the right photo.

    If you can customize the PCB using…

  • RE: A couple of questions for external device values of AD8334

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Simulating AD8333

    Hi Hetashri,

    OK, understand, and I've heard this before. I actually don't have Multisim, ADI has changed to ADIsimPE. However we do have some SPICE experts to support such questions as yours. BTW  there is an LVDS driver shown in the AD8333 data…

  • phase shifter

    Hi i want to buy a phase shifter with following specifications (1)Frequency range: 10KHz to 1MHz. (2)Phase shift:+/-90 degree only, (3) Power: 1-10W. for this i search on many website and at the last i found AD8333 EVALZ board which may fullfill my requirement…

  • RE: What op amp to use as buffer in ultrasound application

    Hi J,

    Sorry for the delayed response.

    Looking at the "Differential Amplifier" you provided in the link, it is actually a difference amplifier (subtractor) and not a fully-differential amplifier. Are you trying to implement a Differential-to-Single-ended…

  • RE: 我想设计一个差分探头,请提提建议

    差分探头主要用于观测差分信号。

    差分信号是相互参考、而不是以地作为参考点的信号。普通的单端探头也可以测量差分信号,但得到的信号与实际信号相差很大,有可能出现“地弹”现象。可选用adi差分放大器

    AD8331/AD8332/AD8334:带前置放大器和可编程输入电阻(RIN)的超低噪声VGA

    实现差分探头差分信号放大

  • AD9277 in die form?

    We would like to use AD9277 for a new design, an ultrasonic test equipment for
    material testing. High integration level and space saving are important aspects
    therefore the preferred component would be AD9277 in bare die (if available),
  • AD9287低温采样噪声问题?请帮忙

    hi ADI专家,

    signal chian: analog input-<AFE-<AD8334-<AD9287-100-<Xilinx FPGA.

    Clock input:epson100M crystal oscillator from TI CDCV304 clock buffer.

    1.8V analog and digital power all from TI TPS5430, analog and digital are from one supply…

  • FAQ: What types of products need VGAs?

    Q.

    What types of products need VGAs?

    ------------------------------------------------------------------------------

    A.

    VGAs are used across a broad spectrum of products and applications. Many high tech comforts of society wouldn't exist without…