FAQ
Hi,
I can't find AD8332-EVALZ Design Files (including gerbers) and 3D step model for the board on the web. I would appreciate it if you could provide them.
Regards,
Ivan
Dear sir,
I designed a schematic by using AD8332 for Automatic gain control. In my card i am not able to achieve the gain of 0 do 48 dB by this IC. Instead i am getting 5 dB overall loss.
I have followed the same which is mentioned in evaluation board…
Hi Dibyendu007,thank you for your reply.
I have tied VCC to SDN pin,and I will go to see if SDN is soldered.
Regards,
Brucelin
Hi,
Is possible to chain the output of channel 1 to the input of channel 2?
What are the considerations I have to take into account?
Regards,
Hello,
I am using AD8332 for low frequency NMR. RF part of my board closely resembles the evaluation board for AD8333. The difference is that i use onboard signal splitter for LNA from minicircuits SCP-2-1-6+, and connect LNA to VGA. Post-detection amplification…
Hi.Our team is developing new products on ultrasonic testing. We chose AD605 as the receiver VGA chip. However, we met a problem as the picture shows: Ultrasonic pulse would make the receiver overshoot although we have designer protection circuit before…
目前AD8331或者一路AD8332的增益调节范围(48dB)无法满足我的需求(60~80dB),尝试了一版电路,将AD8332一路LNA+VGA输出直接接到第二路的VGA输入上,效果不好,噪声较大,请问这样串联是否合适?打算再试一试第一路LNA+VGA输出直接接第二路LNA+VGA上,请问是否可行?或者有其他方法拓展8331的增益范围吗?不是很想继续用经典的两路AD603串联的方法了。急需大侠帮助,先谢谢了!