• AD8305: Measuring low frequency signals

    How can we reduce the bandwidth of the AD8305 to get the average power of a
    modulated (rectangle signal) source in the kHz range? It is no problem to get
    the average power of a HF modulated source (e.g. 52MBit/s fiberoptic
    transmission…
  • AD8305-EVALZ BOM and layout

    Hi everyone,

    I am currently working on a project using the AD8305. Can I request for the BOM of AD8305-EVALZ as well as its native layout and its PDF version?

    thanks and best regards,

    Ahbie

  • RE: AD8304 Using translinear amplifier for low voltage current sensing (100nA 10mA)

    Greetings Hoel-2,

    AD8304 along with the newer release ADL5303 both can only measure current being SOURCED into the input pin. Virtually all input current flows through the NPN logging transistor seen in the IC block diagram, then out to ground pin. By…

  • Current Mirror for ADL5304

    What will be the current mirror if it is needed before ADL5304? The current mirror ADL5315 can only work with AD8305/ADL5303, right? What will be the the minimum detected current if current mirror ADL5315 is connected with ADL5304? Does it have other…

  • RE: Questions about the alternative possibility of ADL5310 and ADL5303

    Sorry about the typo, above. Described spec-by-spec is how ADL5310 and ADL5303 compare.

    Also,

    If ADL5303 is not a replacement for ADL5310, please recommend a replacement part.

    ADL5310 is more like a dual version of the AD8305. Some specs like…

  • RE: RF power detector for very small changes in signal

    I think that you may be better looking at an active detector because they have much better sensitivity. AD8310 (www.analog.com/ad8310), can sense levels down to around -80 dBm which is around 22 uVrms. This is a voltage measuring device. Another option…

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • RE: LT3571 APD Bias circuit

    The LT3571 is used to generate a bias voltage for the APD diode. From the schematics shown on the datasheet it seems this is used for DC level power sensing and to control it's gain but not necessarily as a fiberoptic data receiver.

    I assume you…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…