I want AD8283.cfg for EVAL-AD8283 Evaluation Board.
How should I do to get the latest application?
Hello,
The input impedance of AD8283 can be selected between two values of 200 Ohm and 200 kOhm. Considering the fact that this is actually the input impedance of the LNA block at the front end, my questions are as follows:
- Why is the impedance selectable…
Hello,
We are trying to make use of AD8283 in a radar system. I have two questions about the power consumption in special situations as follows:
1) If only one channel is active, what will be the DC current consumption? DC Currents are given only for…
Dear Sir or Madam,
We are trying to use the AD8283 Evaluation Board with ZYNQ ZC7002 Evaluation Kit. To connect the two boards an interposer board such as CVT-ADC-FMC-INTPZB seems to be suitable. Will you please verify whether or not this adapter board…
Hi,everyone ! Recently, I used a home-made AD8283 board together with original HSC-ADC-EVALCZ to capture signal. A problem was observed that when DSYNC, D0-D11,CLK+ and CLK- connected to HSC-ADC-EVALCZ, the CLK was interferd by DSYNC,and D0-D11( DSYNC…