• AD8283

    I would like to use your analog front-end AD8283. However, i am facing some
    problems looking at the datasheet. The filter cut-off frequency can not be set
    exactly to the sample rate / 2 via the register 'FLEX_CHANNEL_INPUT'. Is it …
  • [AD8283 and HSC-ADC-EVALC]

    I bought AD8283 and HSC-ADC-EVALC as shown in https://wiki.analog.com/resources/eval/ad8283_5cp-ebz

    I have to get the data from not only channel A but also channel B.

    However, the provided GUI can not read the data from channel B.

    I hope the method of…

  • AD8283 gain adjust

    Hello,

    We have AD8283 and we use 4 channels. We want to set flex_gain_1 register to 34dB mode for all channels. When we control the output of adc, we saw A channel is set to 34dB but other channels do not effected that.

    Thanks for reply. Best regards.

  • Can AD8283 be applied as TIA(trans-impedance amplifier)?

    Hi, I am trying to use AD8283 as an amplifier and ADC for visible light communication system. The signal of the silicon photodiode is usually amplified by TIA, but this is the first time I have used such a highly integrated IC. I wonder if the 6 LNAs in…

  • RE: AD8283.cfg and AD8283.cal files ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8283

    Hi,

    I have bought an AD8283 and a HSC-ADC-EVALCZ data capture board. Both are working well, but I will need to make some minor change to the FPGA configuration so that it will work as a DSP system.

    I have looked up your ftp website, there are some source…

  • AD8283

    AD8283

  • RE: AD8283

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8283/AD8285 input current noise

    Hi,

    Is there any ballpark data on AD8283/AD8285 input current noise density available?

    Datasheets, understandably, only specify voltage noise as AD8283/AD8285 are supposed to be driven from low-impedance sources

    Best regards,