• AD8279 difference amplifier - Vref pin

    Hi,

    I am using the AD8279 difference amplifier and am looking to add an offset voltage using the Vref pin. The datasheet recommends using a an OP1177 amp as a buffer between the Vref pin and the reference voltage. Can I use one OP1177 to provide the…

  • RE: I have a problem with AD8279. Please help.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: LTC6810-1

    Thanks Abhishek,

    Yes, I see what you're saying as I looked more closely at my concept, my bad.  I'm wondering if I might be able to create the "string" of smaller attenuated differential voltages using an array of difference i.e. "funnel…

  • RE: PSpice model of AD8273 amplifier

    Hi abhijitpethkar,

    I'm sorry for the delay in answering.

    If this is still a concern, I know of one functional equivalent that has a spice model: AD8279. But the AC specifications are very different. I'll move this message to the Differential Amplifiers…

  • RE: How do I design an attenuator using OpAmp?

    Hi Naji,

    In addition to the considerations that Harry has given, you can also take a look at our AD8275, which is a G=0.2 difference amplifier. With a 0-10V input, it will give you a 0-2V output (or you can level-shift the output) so it won't give you…

  • RE: Request arecommended ADC PN for both porpose Thermocouple and Analog signal

    Hello,

    I receiver your answers about this request through CIA.ASIA.

    Thank you for your help.

    Regards,

    Se-woong

    PS. For you reference, I attach your answers in below.

    ------------------------------------------------------------------------------…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI公司解决方案通报—放大器IC

    目录

    • 差分放大器采用单电源驱动1.8 V ADC
    • 电流检测放大器实现最大1μV/°C的失调漂移性能
    • 经过测试的电路设计
    • 热电偶放大器简化设计
    • 放大器IC选型指南
    • ADC驱动器提供快速压摆率
    • 同类最佳的电压反馈型放大器
    • 输出驱动器增强灵活性和性能
    • 差分放大器驱动184 MSPS SAR ADC,接受±10 V输入
    • 高分辨率、零漂移电流检测放大器
    • 适用于高精度设计的微功耗基准电压源
    • 精密放大器针对低功耗、宽电源电压范围应用而优化