• AD8277 Absolute Value Circuit Distortion

    Hello, I'm trying to build Absolute Value Circuit as described in your application note here Your Absolute Value Circuit, with the AD8277. I was expecting to see a clean rectified wave but it turns out i get significant distortion even at 1kHZ and…

  • AD8277/AD8276 overvoltage/max input current

    Hi,

    We are using a AD8277 Unity-Gain Difference Amplifier and noticed that some parts spontaneous  break down which results in a short on their power pins.  I suspect this happens when a ungrounded device is connected to the inputs. This device floats…

  • RE: Advice on Implementing a Precision Full Wave Rectifier

    Hi David,

    Sorry if we missed this thread. Please see below for my answers.

    1. The AD8277 is a difference amplifier with four on-chip resistors that are laser trimmed for excellent gain accuracy and CMRR. The "R": in figure 3 is the on-chip resistor…

  • RE: Is it possible to precision rectify a 1MHz signal?

    It is always nice to be able to answer one's own questions, since it usually means, that the effort to find out has been succesful.
    I tried to build the circuit mentioned in this publication:

    http://www.analog.com/library/analogDialogue/archives/44…

  • gain reduction of opamp at high frequency

    Hi,

    We are using opamp IC AD8277 along with AD8479 for one of our applications.Upto certain frequencies(7khz)the output amplitude is obtaining somewhat correct as per the gain.But as the frequency is increased,the gain is getting reduced.Can you please…

  • RE: May I use IA in this way?

    FormerMember
    FormerMember

    Adam,

      I can't find AD8577??  Did you mean AD8277??  AD8677??

    Harry

  • RE: AD8276 output capacitive load drive capability

    The AD8276 (and AD8277/78/79) can drive ~200pF without adversely affecting settling time and overshoot.  You can drive a higher capacitive load, but it may increase the settling time and overshoot.  Or you can add a small resistor (~20 ohms) in series with…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI公司解决方案通报—放大器IC

    目录

    • 差分放大器采用单电源驱动1.8 V ADC
    • 电流检测放大器实现最大1μV/°C的失调漂移性能
    • 经过测试的电路设计
    • 热电偶放大器简化设计
    • 放大器IC选型指南
    • ADC驱动器提供快速压摆率
    • 同类最佳的电压反馈型放大器
    • 输出驱动器增强灵活性和性能
    • 差分放大器驱动184 MSPS SAR ADC,接受±10 V输入
    • 高分辨率、零漂移电流检测放大器
    • 适用于高精度设计的微功耗基准电压源
    • 精密放大器针对低功耗、宽电源电压范围应用而优化