AD8275的压摆率是多少V/us?
一个1kHz~1MHz的正弦波信号,该芯片能够处理?会不会速率达不到?
Hi,
I would like to know that is the absolute tolerance of the 50k ohm resistors inside the part.
Thanks;
Leo
Is there any suggested reflow profile available for AD8275?
Just placed 100 and 3 are not working.
The AD8275 is a level translator with rail-to-rail output.
But if this is true why is there an output swing ?
OUTPUT CHARACTERISTICS
Output Swing
(VREF2 = 4.096 V, REF1 and RL connected to GND, RL = 2 kΩ)
−VS + 0.048 +VS − 0.1
I want to use this…
I want to use AD8275 for attenuating the output from sensors varying from -10V to +10V, before giving to ADC.
Is AD8275 meant to use only for driving 16 bit successive approximation ADC? Is it possible to use AD8275 for driving 24-bit ADS1220, which…
AD7685+AD8275 对于参考电压REF问题
AD7685[pin1]+AD8275 [pin8]之间 输入一个参考电压源ADR391。我们使用标准的电压信号
+/-10V输入。经过AD8275之后缩小0。2倍后,再加上参考电压源ADR391,2.5V。在AD7685 输入端就变成了2.5V+0.2×Vin;这时,A/D转换器AD7685 采集电压范围从2.5V~4.5V之间。AD7685量化的电压范围只有0~2V。而且,采样数据只有0x3000 ~0x7FFF 之间。量化的数据范围减小了一半…
In Page 4,
10db5e82155a64e37b53bc76c9735de4.html
I think the Vout here should be Vload, or (Vout - Vs/2).
Is that right?
Thanks,
Vic