问题:AD8274输出直流点产生偏移,理论上Vout的直流量应为2.5V,实测结果为3.3V,且在输入端口施加小信号激励时,输出没有任何变化; 测试条件:对AD8274 Vin+和Vin-输入为2.5V,REF点为2.5V,Vs+为5V,Vs-为0V按照AD8274参考手册中图40的方式连接,增益为0.5;
问题:AD8274输出直流点产生偏移,理论上Vout的直流量应为2.5V,实测结果为3.3V,且在输入端口施加小信号激励时,输出没有任何变化; 测试条件:对AD8274 Vin+和Vin-输入为2.5V,REF点为2.5V,Vs+为5V,Vs-为0V按照AD8274参考手册中图40的方式连接,增益为0.5;
Hi,
I'm using the AD8274 to measure the voltage of a cell (2V to 5V), with a 0V +7V supply voltage, coming form a buck converter. I'm using the G=1/2 configuration.
It looks the maximum common-mode voltage I can apply is +16V, then the output…
The AD8274 is specified at ±15 V, but it can be used with unbalanced supplies, as well. For example, −VS = 0 V, +VS = 20 V. The difference between the two supplies must be kept below 36 V
数据手册中这段话不是说明了AD8274在负电压是0V时,正电源小于36V就可以工作吗?,我使用5V供电…
Looking at the specs, in particular figures 8 and 10 on page 6, the common-mode voltage seems to be limited to 25V for +/-15V supplies.
My question is: where is that 25V measured? At the pins of the IC, or at the inverting and non-inverting input pins…
我发现文档CN0116里给出的参考原理图里,AD8274的管脚顺序和AD8274的数据手册里给出的不一致,8274里数据手册上引脚2和3是输入端,而CN0116里成了1和6是输入端,想问问ADI工程师,这是不是文档的一处错误,哪个是正确的,谢谢
Hi,
Thank you for your recommandations.
Actually i would like to you use AD8274 or AD8271 difference amplifier.
Should i use buffer amplifier (like LT1818) at inputs?
前不久,斑竹为大家整理了2021年论坛热门技术帖的上半部分,还没参考的小伙伴可以点击这里回顾哈→ 论坛工程师原创——2021年论坛热门技术帖(上)!
今天,下半部分上线!赶紧收藏呀~
------------------------------------------------------------
ADA4817做光电二极管前置放大电路问题
https://ez.analog.com/cn/amplifiers/f/q-a/544080/ada4817
芯片选择:输出60Hz方波电压…
Original Question: encrypted models for amplifiers by timothy.starr
Hello
We are currently running 7.2, but can not simulate ourentire circuit due to node restrictions.
It seems that ADA4817, AD8274 and ADA4937 are not encrypted. Are there any plans to…
Hi mohammadsdtmnd,
The AD8333 can still be used in your design by using the block diagram seen on Figure 53 of the AD8333 datasheet, you can used the AD8282 as the LNA for the input of AD8333 and use AD8021 as the TIA and summer to convert the output current…