AD8273 Datasheet 第四页,ABSOLUTE MAXIMUM RATINGS 中 Voltage at Any Input Pin这个参数是40V,而其他同系列的都是-Vs+40V,AD8273的这个数据是不是错的?如果不是错的,那么与Figure 9的区域存在矛盾,两个中里面应该有一个是错误的analogchina-admineazone
AD8273 Datasheet 第四页,ABSOLUTE MAXIMUM RATINGS 中 Voltage at Any Input Pin这个参数是40V,而其他同系列的都是-Vs+40V,AD8273的这个数据是不是错的?如果不是错的,那么与Figure 9的区域存在矛盾,两个中里面应该有一个是错误的analogchina-admineazone
AD8273共模电压范围疑问
根据datasheet 第3页,Vs=正负15V,
Input Voltage Range |
-3VS + 4.5 | +3VS - 4.5 |
计算输入范围为-40.5V~+40.5V;
但是第6页
Figure 9的曲线又改怎样理解?共模电压不能超过正负25V? 应该以哪个为准呢?
|
I required the PSpice model of the AD8273 but as it is not available on the website. Can you possibly provide me the nearest equivalent PSpice model of AD8273?
If the nearest equivalent model is not available can you let me know how to simulate the above…
Hi,
I am designing a conditioning circuit for a MEMS analog microphone and I would like to use an IC for single-ended-to-differential conversion in order to have a balanced line output capable of driving twisted-pair cables. I found that the difference…
Hi mehran.rizi@bd.com,
Thanks for running the experiment.
I've seen some instability issues resolved by adding a series RC shunt to the output. This will have no effect on your low frequency / DC accuracy.
Also, I wanted to point out to make sure…
Original Question: AD633 using ADIsimPE by crlMIDI
I tried to simulate the voltage-controlled quadrature oscillator of the AD633 application note, using ADIsimPE, but it said there are too many analog nodes. I note that the model for this fairly old part…
Hi,
I'm designing a circuit around the AD977XA series (specifically, the AD9778A) of high-speed DACs. I'm not too experienced so wanted to get some general feedback/background/context on the output stage. I will be updating the AD9778A at 50 MHz and…
Hi Naji,
In addition to the considerations that Harry has given, you can also take a look at our AD8275, which is a G=0.2 difference amplifier. With a 0-10V input, it will give you a 0-2V output (or you can level-shift the output) so it won't give you…