• AD8253 PGIA nose issue

    Dear Sir,

    The PGIA AD8253 datasheet showed noise performance:

    Voltage offset RTI Vos +-150+900/G uV.

    Voltage nose 0.1~10Hz,RTI,G=1, 2.5uVp-p.

    Then I tested AC performance by 6.5 Digital MultiMeter(HP-3304A), which noise performance showed 4.03mV DC…

  • AD8253 excessive bias current

    Using AD8253 in classic scope-type DAQ front end. Both inputs have 1 Mohm to ground. In an AC-coupled mode, the amp Ib develops offset voltage across the input resistor. Data sheet specs indicate 5 nA typical, 50 nA max over temp, further supported by…

  • AD8253 output short-circuit current definition

    AD8253 DS In page 6, the “Output Short-Circuit Current”
    Is specified to be Indefinite.
    This means unkown, un-tested or can be very large?

     

    It would probably be better if we said:
    Output Short Circuit Current Duration:  Indefinite
  • AD8253  AC耦合问题

    按照数据手册所示设计一个10hz-25khz的交流耦合输入。所选电容为4.7uf,电阻为1M欧姆。电源供电为±12V。在实际的测试中,发现SFDR比较差,在15-25DB范围,如果采用直流耦合的话,SFDR在60DB以上。做了这样一个测试,将AC信号输入,在RC的输出端,运放的输入端引出两根线来分析,发现SFDR也在60DB以上,但是AD8253的输出端得到的SFDR就很低

  • AD8253 spec under +-5V power supply

    Here is one customer wants to know the specification of AD8253 when use +/-5V
    power supply. However, the spec table in datasheet is only for +/-15V power
    supply.

     

    The specifications at +/-5V should be nearly identical to +/-15V
  • Whats about AD8253 PSpice model?

    I would like to try in practice AD8253 psice model ( .cir file ) from product details page ( http://www.analog.com/en/specialty-amplifiers/instrumentation-amplifiers/ad8253/products/product.html ). After import of this model to cadence orcad I found that…

  • AD8253供电问题

    AD8253能通过以下供电方式供电吗?

    其中AD8253的负电压(VS-)是由一个运放(AD8597)将正5V转为负5V而得到的。

    采用这种通过运放反向而得到负电压来供电时,出现了以下问题:当在AD8253的 Vi+(AD8253的10引脚)输入一个几十KHz的正弦信号时,其输出为一个周期为几十纳秒的正弦波。且AD8253的增益控制出现了问题。

    若采用一个电荷泵将正电压(+5V)转换为一个负电压(-5V)给AD8253供电,则AD8253的输出正常,且其增益控制正常。

    由于电荷泵输出的负电压的纹波太大…

  • ad8253供电问题

    我采用AD8253做一款放大电路,输入信号均为mv级,输出在0-5V范围内,由于电源设计原因导致正负双电源不对称,如正电源为﹢8v,负电源为-6.5v,想咨询一下,这种不对称供电是否对信号有影响。另外,不对称的供电方式是否对输入信号的或者输出信号产生一个直流偏量。

  • AD8253可控增益问题

    请问为什么使用锁存增益模式时,控制使AD8253增益为100时出现错误?以下是电路板的原理图


      
    就用这一原理图,用单片机控制时AD8253的增益分别为1和10时都没问题,但控制使其增益为100时却出现了错误,增益变为1了。我将原理图中的C2去掉,也即将AD8253的输出与下一级的AD8597断开后,再控制使AD8253的增益为100,则没问题,其增益变为100。而在Transparent Gain Mode模式下,100增益则无问题。

    还有就是请问如何产生一个精密的负电压 -5V 给AD8253供电啊…

  • ad8253增益不能控制

    按照CN-0359原理图设计的方案,现在ad8253增益不能控制,而且2片ad8253都发热啊?ADA4627也发热!不知道是什么原因?请帮忙分析!A0,A1,WR的高电平是3.3V 低电平是0V。谢谢!还第一次遇到运放发热的!