• Questions about AD8253/AD8251/AD8250 ?

    Hi,

    I wonder if it's enough for AD8253/AD8251/AD8250 to output ±10V when it is supplied with a power of ±12V ?

    Thanks.

  • SNR of AD7768-1 with AD8250 at 48 kHz input frequency

    Hello,

    my customer asks for the SNR that is to be expected with the following signal chain:

    48 kHz input-signal ---> AD8250 ---> LTC6363 ----> AD7768-1

    AD8250 is powered by +/-15 Volt.
    The LTC6363 translates the up to +/-10V output from the AD8250…

  • Could I have AD8250 model file?

    Original Question: Could I have AD8250 model file? by moto

    Hi

    I want to do the simulation of AD8250.

    I made the model from "AD8250.cir" file.

    But I couldn't simulate that.

    Error message is below.

    *** ERROR *** The circuit is too large to…

  • Where is LTspice model of AD8250?

    Anonymous
    Anonymous

    Hi

    Question is very simple.

    I have tried simulation of AD8250 Instrumentation Amplifier in LTspice.

    Spice model of AD8250 gives failure results in LTspice environment.

    Have you got correct LTspice model of AD8250 chip?

    Regards

    Andrzej

  • RE: AD8250 Reference Drive

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8250 - AD8253 spice model LTspice results

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8250 output voltage offset differes from reference input

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8250 电容耦合输入   输出有大的偏置电压

    This question has been closed by the EZ team and is assumed answered.
  • RE: Overvoltage Behavior of AD8250

    Hi Chunlee,

    Apologies for the late reply. By applying +20V input to its IN+, you are saturating an internal node of the in-amp which invalidates the output. By operating outside the valid operating region, the device will not work as expected. You can…

  • Cascading a AD8250 and a AD8253

    I want to build a high variable gain amplifier and have cascaded a AD8250 and an AD8253 in order to have the gain to vary in the 1, 2, 5, 10, 20, 50, 100, 200, 500, 1000, 2000, 5000, 10,000.

    However, I have experienced a strange distorsion for low amplitude…