I'm looking for a unity-gain, low-power op-amp to replace an AD8244 as a voltage follower. I only need one amplifier circuit (not the four that the AD8244 has) and care about low cost, low current draw, ability to run on a single-ended 3.3 V supply…
I'm looking for a unity-gain, low-power op-amp to replace an AD8244 as a voltage follower. I only need one amplifier circuit (not the four that the AD8244 has) and care about low cost, low current draw, ability to run on a single-ended 3.3 V supply…
I am doing some active filtering and I am looking for what will work best for my application. I had someone recommend the AD8244. When I go to the filter wizard it doesn't even give the option for the AD8244.
The project is I have to put a high pass…
Hey, I am having trouble with using the AD8244 for buffering a RC high pass filter. As I saw the datasheet describes creating a sallen-keys filter I figured this chip would be a great option - particularly as I need to do this for 32 channels, the reduced…
1.Is it possible to make high input impedance circuit ecg acquition (to overcome for mismatch between source impedance of different leads, working against the input impedance of the front-end amplifier ) using ad8244
2.please give me the application circuit…
I plan to use AD8244 as a input in an EEG amplifier. Using AD8244 I can achieve extremally high DC-impedance (resistance), but the capacity is still 4pF. 4pF paralelly with 10TOhm for 10Hz (alpha band in EEG) degrades DC-impedance a lot.
Is it any possibility…
Yes, RLD = Right Leg Driver.
I want to use AD8244 as input buffer and Low-Pass Filter for EEG device. But I'm not sure, can I use AD8244 as RLD?
1.Is it possible to make high input impedance circuit ecg acquition (to overcome for mismatch between source impedance of different leads, working against the input impedance of the front-end amplifier ) using ad8244
2.please give me the application…
Hello,
I'm trying to find solution for EEG measurement (1-channel).
According to EEG application note, below components are recommended.
- AD8220(AMP), AD8244(Buffer), AD8422(AMP), AD7768-1(ADC).
1. Can I use AD8244 without AD8220 to connect electrode…