• RE: Reducing RFI on AD8223

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: RFI problem about AD8223

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Setting up circuit with AD8223

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: PSPICE Simulation Model for AD8223?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8223 gain issue

    Hello every one!

    In my design, I am using a AD8223 as a current sense amplifier on a +5V 10A power supply.

    Here is the AD8223 wiring:

    -Vs = GND (0V)

    +Vs = +15V

    REF = GND

    RG = 1.23kohm

    IN+ and IN- are connected to the sense resistor, which is in…

  • AD623_error output under stress

    One of our customers meets an issue of AD623, Could you give any suggestion?
              The power is 3.3V single supply, REF pin is 720mV, Gain resistor is
    470Ohm, Gain is about 210.
              When he twists the board, the AD623's output will also change…
  • RE: Alternative to AD623

    Hi Wbadry,

    The next generation of this part is the AD8223. I would like you also to check out the AD8422 which is a high performance, low power, rail to rail amplifier. It has better overall specs than the AD623 and AD8223..

    I hope this helps.

    Best regards…

  • ADPD188GG PPG

    I am preparing a smart wearable medical product for the elderly.I have some questions about ADPD188GG, and I look forward to your answers. I will to test the CNiBP, SpO2 and HRM / HRV of the elderly.so,

    1.   CNiBP :   AD8223+ADPD188GG, connected to PD1…

  • Absolute max supply voltage rating AD623

    Hello,

    I'm working with the AD623 and powering it from 12V, which is the top of the power supply operating range (2.7 - 12V). However the absolute maximum supply voltage rating is ±6V (or 12V) so there is no margin between the two.

    I'm assuming…

  • RE: 【每周一答】微信题目跟帖处(最后一波)

    3年,AD8223+山野樵夫+《你好,放大器》