• AD8215 Negative Current

    Good day,

    Can the AD8215 handle a negative sense current, i.e. what is the maximum negative differential voltage the AD8215 can handle between the IN+ & IN- pins?  I could not find a clear answer in the datasheet.

    Application:

    I'm using the AD8215…

  • AD8215

    I have some unclear questions needed to clarify with you.

    1. 1)      Do you have any application note for using current sense amplifiers, what are the errors that needs to be factored in, etc.
    2. 2)      Any spice simulation tools recommend for AD8215?
    3. 3)      What…
  • AD8215 No Connect...

    I'm switching from a AD8210 to an AD8215 in my configuration.  I have pins 3 and 7 (Vref) tied to ground when using the AD8210 device.

    The AD8215 lists pins 3 and 7 as no connect and I have them tied to ground.  Is that going to be a problem?

    Thanks…

  • RE: AD8210检测电流大小问题

    单向电流检测的情况,应该让R上的电压在电流最大的时候不超过250mV,注意要考虑可能出现的最大电流,而不是需要测量的最大电流,另外还需要留一些余量。

    AD8210是双向高压采样期间,如果只要单向可以考虑AD8215,如果不需要高压,也有更便宜的器件。

  • External input filtering effect on high side current sensors such as the AD8210?

    What are the limitations to adding input filter resistors to high side current sensors such as the AD8210?

  • AD8227 output voltage limitations @ 0..100mV CM input

    1.
    I am considering using your AD8227 instrumentation amplifier to replace an
    existing part. The existing part is unable to drive sufficient output voltage
    at the common mode input voltage I have. I have a common mode input voltage
  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…