Good afternoon, I can't find any information about pins forming for creating footprints in Mentor Graphics. Would you be so kind to help me? Best regards Andrey
Hi,
Could you please share the AD8212 pspice transient and average models?
I'm using AD8212 to measure current through led lamp.
The dropout voltage on R15 is 0V i don't know why.
See attached schematic and PCB layout.
there is no connection between GND_ISO and GND_48V.
pls help.
tnx
Hello,
I didn't find any information about which is the maximum differential voltage the amplifier can sustain without any failure in the datasheet. In this site, I found a similar question but referred to the commercial part. The answer was 2V.…
Could you please releash the transient and average pspice model of AD8212?
I didn't find any information about which is the maximum differential voltage the amplifier can sustain without any failure in the datasheet. In this site, I found a similar question but referred to the commercial part. Th answer was 2V.
I am going to measure up to 10A using a shunt of 10milli-ohm.
I am amplifying the voltage across the shunt (which is 0mV to 100mV) as Vsense using AD8212.
The real problem i am facing while my Vsense is less then 20-25mV.
I would like to hear any…
I was looking for a current sense amplifier with a high common mode voltage and I saw your circuit from the lab CN0218 which showed how you can achieve more than 500V of common mode voltage with the AD8212. In my design I have a source that is…
Hi there,
I have some question's about AD8212 for monitoring high voltage.
According to the datasheet, it says that "7 V to >500 V with external pass transistor ".
#1,Why is the common voltage limited upt to >500V ?
#2,Is it possible…
Hi all,
I have a prototype circuit board to test AD8212 for 100V application. Circuit is shown below.
I apply Input DC voltage and draw DC current. When i changed the input DC voltage step by step, while drawing same DC current at output, I cannot obtain…