Where is mistake?
20 ohm Resistor between v+ and shunt or between V- and shunt could be damaged.
We are checking motor drive current by AD8211. Motor VCC 24V and GND (GND_Motor) is filtteres (Emifilter)
AD8211: V+ is connected 5V_CTRL (using cap 100n…
最高电压为21V的1A线性恒流电路中做高端采样,采样电阻0.1欧,AD8211供电5V。有时候负载断开再接入,AD8211会损坏,芯片发烫,已经烧掉好几片了,这种情况怎样避免??
Has anyone observed difficulties with AD8211 during BCI EMC testing in the 800MHz to 1.5 GHz range? Device is configured as current sense amplifier in PWM solenoid driver. Sense resistor is located between coil and low-side FET switch.
i am using ad8620 configured as a differential unity gainbuffer feeding a ad8221 instrumentation amplifier
the ac signal (100hz to 100khz) is fed to two resistors inseries
aim is to measure 1m ohm to 100M ohm
sense resistors are 100R, 1k, 10k ,…
Hi !
I have some questions about ADI datasheet.
Our team are checking the datasheet because if the datasheet was changed we have to explain the changes.
And today , we found many datasheet was changed.
For just one example , AD8206 datasheet was changed…
Hi,
**EDIT** I read that my original part AD8211 is a unidirectional current shunt monitor, so now I have revised the question using a bidirectional chip the AD8418. Question has been re-written with AD8418.
I am confused to whether the AD8418 (current…
你好,使用AD8211检测28V,8A电流,AD8211供电5V,分流电阻使用0.01欧姆,上电后烧冒烟了。检测2A左右电流没有问题。请帮忙分析一下原因,感谢!!!