• RE: (AD8417)If I can calibrate the system , can I cancel the input offset?

    Hello Kawa,

    If you have a way to disconnect the high end of your resistor from the source (maybe a switch), then it does look like you could calibrate that error our correctly. What you get out of the ADC in that condition should be the error that you…

  • RE: 有奖征集丨工业技术千千万,你想Pick哪一款?

    智能环保汽车/ADI汽车传感器和传感器接口解决方案

    车辆中通常 有超过100个传感器,通常按功能可以分为6类,包括压力传感 器、电流传感器、电容传感器、位置传感器、速度传感器和温度传感器。车辆传感器可用于传动系统、底盘/安全和车身系统。

    (1)ADI公司的应变信号调理IC ADA4557是一款单电源桥式传感器信号 调理器,额定温度范围为−40°C至+150°C,采用4 mm × 4 mm小型 LFCSP封装。

    (2)ADI电流检测放大器AD8207/AD8208…

  • RE: LTC6102 or Other Recommendation

    Hi ,

    In case you've not seen our parametric search for Current Sense devices, here it is.

    You can use the Excel filters to narrow down your search.

     XLSX

    Regards,

    Hooman

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI汽车传感器和传感器接口解决方案

    ADI汽车传感器和传感器接口解决方案

  • ADI公司解决方案通报—放大器IC

    目录

    • 差分放大器采用单电源驱动1.8 V ADC
    • 电流检测放大器实现最大1μV/°C的失调漂移性能
    • 经过测试的电路设计
    • 热电偶放大器简化设计
    • 放大器IC选型指南
    • ADC驱动器提供快速压摆率
    • 同类最佳的电压反馈型放大器
    • 输出驱动器增强灵活性和性能
    • 差分放大器驱动184 MSPS SAR ADC,接受±10 V输入
    • 高分辨率、零漂移电流检测放大器
    • 适用于高精度设计的微功耗基准电压源
    • 精密放大器针对低功耗、宽电源电压范围应用而优化