• AD8203 Θja

    Hi 

    Can we know Θja about AD8203YRMZ-R7?

    Best regards 

  • I want to use AD8202 and AD8203 properly

    I want to mount AD8202 or AD8203 on the same print pattern and create a board with a gain of 7 and a board with a gain of 10.
    The connection between Pin 6 and Pin 7 is an obstacle, but isn't there a good idea?

    Best regards

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    我又来了!再签到!

    北京,朝阳区,工业控制,关注AD8202 AD8203 AD8205。

  • Single ended op-amp with an adjustable common mode

    Hello,

    We are looking for an op-amp with an adjustable common mode, in order to implement a single supply amplifier.

    I could easily find a lot of fully differential amplifiers with adjustable common mode, such as the AD8137 that we used before, as well…

  • RE: ADF4351. Phase change at the output for a given law.

    The phase of these synths should not change once set.

    For more information please check the attached article.

  • RE: Output signal phase ADF4351

    In answer to the first query, since this part is a Fractional-N, then the phase between REF and RFout can vary, considerably. However, using phase re-sync and fractional-N it is possible to get repeatable phase at the RF outputs.

    The attached article…

  • RE: Phase Coherent When Frequency Hopping of ADF4350

    Hi,

    The attached article detais the implementation of phase coherency.

    Ian

  • ADF4350 Phase Resync

    Ths is comment on recent posting of an App Note

     

    Achieving phase coherence between multiple Fractional-N PLLs

    ADF4350 Phase Resync and Phase Programmability

    Please post the two references cited as hyperlinks - 'here' - I could not click into them…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…