• About AD8192

  • AD8192 DDC buffer architecture

    Dear Sirs

    1. For AD8192 DDC buffer architecture : Is SVO architecture or others?

    2. Can AD8192 DDC buffer Cascaded different DDC buffer?

    BRS

    Nat

  • AD8192 HPD pulled low

    Specs mentions "Hot plug detect (HPD) signal is pulsed low on link switch.  Does it happen every time I program bit HS_CH either 0->0, 0->1, 1->0, or 1->1?  Or does it happen only when I program with true bit toggling 0->1 or 1->0 ?…

  • About AD8192 I2C glitch

    Hi all,

    good day!

    Our customer has a issue at I2C bus.

    Due to the rising edge has the glitch behavior, so the projecter HDCP function will be fail.

    do we have any solution ?

    eg.

    a. about  I2C pull up resistor and Rs, do we have something suggestion ?

  • AD8192 2K pulldown on CLK(-) of Source Channels

    Can someone tell me why in Figure 30 on page 20 of the datasheet, the CLK(-) signal of each source channel is tied to ground through a 2K resistor?   These same pulldowns are also found on the AD8192 eval board schematic.

  • Ad8192 DDC function

    Dear Sirs

    - The AD8192 if having the push-pull ability? 
    - What is AD8192 automatic switch mechanism?
    BRS
    Nat

  • RE: AD8192 TMDS Output

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8192 display issue

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD8192 DDC bus direction setting

    Dear Sirs

    May I set DDC_A0 unidirectional (left to right)?

    And How I set it?

     

    BRS

    Nat

  • AD8192 Input Schematic for DDC bus

    Dear Sirs

    Could you provide me the AD8192 Input Schematic for DDC bus?

    Thanks