• AD8191 Channel Select

    I have configured the AD8191 for parallel interface, however if I left the channel select (PP_CH[1:0]) disconnected (i.e. floating or high-impedance), would this make Channel "00" the default? 

    Thanks in advance

  • AD8191: Crosstalk and isolation

    I have a customer who is designing the AD8191 into a dual link DVI KVM and need
    to know the isolation and crosstalk figures.

    They are interested in frequencies up to the maximum single link data rate of
    1.65Gbps, but any figures you…
  • RE: DP++ mux with AD8197B or ADV3002

    Hi,

    These two chips are multiplexer not a converter, So i believe it is a passive adapter.
    And both the chips are transmits the data through the TMDS lines.But ADV3002 does not support the dual-mode and single-mode switching functions as like of the AD8191…

  • ADV3002 in KVM

    I am trying to design an advanced KVM and the ADV3002 looks very interesting except for the 1920x1080 limitation.

    In a previous app note I saw mention of using 2 AD8191's to achieve dual link for higher resolutions. Id like to know if the ADV3002 can…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…