• AD8184 Video Mux 4:1

    Regrad AD8184  

    Is it Possible to operate with single supply +5v ?

    Thanks,

    Moshe

  • About AD8184 Cross talk

    Hi,

    My customers are considering using the AD8184.
    I got a question there.

    #1  Is there a crosstalk graph when  the driving input is 1 channel?
      (The other conditions are the same as in FIG. 12)

        I attach a figure as an example as an example.

          (IN0…

  • RE: AD8184 Crosspoint failure

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Demultiplexer equivalent of the AD8184 4:1 video multiplexer

    I am looking for something like the AD8184 except that I would like a demultiplexer instead of a multiplexer.

    In other words, I would like to have a single signal input that can go to one of four buffers.

    Do you have such a component but with the same…

  • RE: Combining 4 analog video input to 1 output to show on Analog Monitor

    Hi,

     Please refer below product page and choose the chipset according to your requirment,

      https://www.analog.com/en/products/switches-multiplexers.html

    Note: AD8184 is a high speed 4-to-1 multiplexer. It offers –3 dB signal bandwidth of 700 MHz along with…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…