• AD8183 for new design

    Hello,

    as AD8183 is release on 1994, is it recommendation for new design?

    Have any new parts suggestion? pin to pin compatible is much better.

  • RE: Can the ADV7403 supports more than two RGB inputs?

    Does the same go for YPbPr with SOY?

    I have an application that requires 4 YPbPr inputs, all with SOY. Would the best option be to use a couple of AD8183 or similar to mux the 4 inputs down to 2? Which input channels would be best to use?

    Many thanks…

  • Common-mode voltage AD9283-100

    Greetings! I have what is probably a dumb question but I want to be sure. The datasheet for the AD9283 says the inputs are biased to 0.3*Vdd (approx 1 volt). I also see that there is a range of +/- 200mv. I plan on driving this ADC with AD8138 (single…

  • RE: AD8138S - Radiation questions SEU and Dose Rate questions

    Hi Dave,

    Notes 5 & 6  at the bottom of page 4 are boiler plate notes on the SMD drawing.

    Analog Devices supplies two models of the space qualified AD8138S devices. The 01 models are TID High Dose Rate Tested to 100Krad in accordance with MIL-STD…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…