• RE: AD8170 noise figure

    The AD8170 appears at the end of a signal attenuation chain.  In signal processing normally one would want to use a LNA before going to an attenuator after an antenna but we are not doing that to due the complexity.  The AD8170 is driving another vendor…

  • Problem with AD8170 spice model simulation

    Folks

    I downloaded spice model of AD8170 from AD official page, but faced with this error when I simulated a simple test circuit in LTSpice.

    anyone knows what it means?

    TanQ

  • AD8170/AD8174 Output Capacitance

    Hi

    I am seraching for a an analog multiplexer with a very low "total" input capacitance value.

    Output capacitance information exist only for AD8174 /"Output Capacitance Disabled (AD8174) 7.5 pF" page 3 of datasheet) when disable so could I…

  • RE: AD8182 simulation model

    Hi Hoang Dao,

    The AD8182 does not have a spice model yet. But for simulation purposes, you can use the spice model of AD8170 attached. It has almost same specs and performance with AD8182, the difference is that it is a single 2:1 Mux, 250 MHz Bandwidth…

  • Video Switch 6:1 with Audio

    Hello everybody,

    I'm searching for a analog 6:1 video switch and if possible with audio. Otherwise I need another IC for doing the audioswitching.

    I found the AD8174 (http://www.analog.com/static/imported-files/data_sheets/AD8170_8174.pdf) but this…

  • RE: AD8302 low frequency design issues

    Tanq for the reply

    About your answers

    1. Ok so I have to test several large caps till reaching proper ripple in low frequencies, is it right?

    2. I have to use an analog front end circuit for conditioning sinwave inputs. Pls consider these notes about…

  • RE: High Speed low noise Instrumentation Amplifier with Disable?

    Hi, wivern.

    I have few suggestions that you may consider for your design.

    1. Your 50ohms resistor is too low to be a load of your in amp. This will dissipate a lot of power. It would be better if you increase the resistance and reduce the 1uF capacitor…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • ADI处理器实用经典著作—《高速设计技术》中文电子版

    本书内容包括三大部分:


    1 部分从运算放大器的基本概念和理论出发,重点介绍了运算放大器的原理与设计,以及在各种电子系统中的应用,包括视频应用、RF/IF 子系统(乘法器、调制器和混频器)等;

    2 部分主要介绍了高速采样和高速ADC 及其应用、高速DAC 及其应用、以及DDS 系统与接收机子系统等;

    3 部分介绍了有关高速硬件设计技术,如仿真、建模、原型、布局、去藕与接地,以及EMI RFI设计考虑等。

    书中内容既有完整的理论分析,又有具体的实际应用电路,还包括许多应用技巧。特别适合电子电路与系统设计工程师…