FAQ
Hi,
It is best to use the parts up to 30V only.
You can also see on TPCs that some of the plots were taken using supply of +/-5V or +/-15V.
The device is operational up to +/-18V but we could not guarantee device performance as it is already hitting the…
I could see from the datasheet that the short-circuit current is 90mA but what is the max duration? In the datasheet, it says 'See Derating Curves'. I don't understand what that means. I am driving capacitive loads directly (16 source pins of AD1434 quad…
AD817的输出驱动能力和ADA4870输入阻抗应没有匹配问题,是否是因为面包板过大的寄生电容导致。可以使用spice仿真确认二者的特性,是否也有如上现象,如果没有建议直接在PCB上验证。
Im using a op amp as the front end for my data acquisition card
Choose the AD817 amp powered with a 12v single power supply
I have a 4v peak to peak signal going into my system
The signal im getting on the output of the AD817 seems to be just the positive…
I Have AD817.cir from analog site, but I have no idea how to use it on LTspice?
there is whats inside it:
* AD817 SPICE Macro-model
* Description: Amplifier
* Generic Desc: High Speed, Low Power Wide Vs Op Amp
* Developed by: ARG / ADI
* Revision History:…