• AD8159: Layout

    What is the recommended power bypassing? There are 5 different types of power
    pins: Vcc, Vtto, vtti, vttio, vttoi.
    1) If I am using AC coupling, can I connect them all to the same 3.3v plane, or
    should I have different plane for each?
    2) What…

  • RE: AD8159 EVAL BOARD SCHEMATIC AVAILABLE??

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Question about Max. Power consumption and  Ψjt of AD8159

    Hello,

    My customer asks maximum power consumption and Ψjt of AD8159.

    Please refer below questions and let me know your answers ASAP.

    1) About maximum power consumption of AD8159

    In a datasheet of AD8159, there are two kinds of power dissipations.

  • Question about a circuit of AD8159 input pins

    Hello,

    My customer is using AD8159 in their system like below.

    (They used a serial connection with 10 nF in front of input pins.)

    And they want to change from 10 nF to 50 ohm for reducing the value of output voltage level like red box in below picture…

  • RE: Thermal data of AD8159ASVZ

    Sorry for the delay in response. The AD8159 is in the same product family as the AD8152. You can refer to the latter datasheet for thermal parameters, on page 8. Copied the excerpt below.

    MAXIMUM POWER DISSIPATION The maximum power that can be safely…

  • RE: AD8192  application issue

    Hi,

    The AD8192 data path is uni-directional and not bi-directional. Therefore, it cannot support the proposed configuration of driving a signal on one input and fanning it out to two outputs.

    ADI does provide network switches like the AD8159 that can…

  • RE: Any 8x8 switch similar to ADN4612 (11.5Gbps per channel)

    Hi Gurusaiprasanth,

    ADI has a series of Digital Crosspoint Switches products, however two digital cross switch products (ADN4612 and HMC857) in the range of 11.5Gbps with different channels. Please refer to the below list of high speed digital cross switch…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225