• Alternatives to the AD829

    Alternatives to the AD829

     

    I can recommend alternatives though. Other single high speed opamps with
    Bandwidth > 120MHz and Slew rate > 230V/us are

    AD811 Single
    AD818 Single
    AD815 Dual
    AD828 Dual

    You will open up…
  • power amplifier

    I am looking for a power amplifier which can drive from 100mA up to 500mA (differential output) into an inductive load (it is just 100uH I guess).

    The design is a servo loop. The loop bandwidth is DC to 100Hz only, but I need all the low noise I can…

  • RE: Does Analog Devices Make This Amplifier?

    Hi,

    Apologies for late reply.

    Here are some amplifiers to consider.

    AD8397 is a rail to rail high output current amplifier capable of driving heavy load while maintaining near to rails output swing. Output positive swing to +11.89 V and output negative…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…