• RE: AD8142, AD8143 reference design

    Hi, Stephan.

    AD8134 is an older version of AD8142 while the AD8147 is the higher version of both the AD8142 and AD8134. These three just differs in some of the specs like the power supply range, -3dB bandwidth, gain and the size of the exposed paddle…

  • RE: AD8145EVALZ and AD8147-EVALZ

    Hi, Venkatesh.

    AD8145 can be replaced with AD8143 which has lower bandwidth. AD8147 can be replaced with the following video drivers AD8134, AD8142 and AD8146.

    Regards,

    Anna

  • RE: AD8145 comparators schematic design

    Hi,

     For resistance details, Please refer https://ez.analog.com/video/f/q-a/7498/ad8142-ad8143-reference-design

     I beleive yes you can,AD8145 is designed to work with dual rails, like +-5  or +-2.5V, not just +5V.  
    Sine the differential input is not AC coupled…

  • AD8134 Help Required

    Hello everyone,

     

    I require to convert RGsB (Gs means "Sync on Green") signals of a Single Ended video stream into Differential output.

    I researched and found AD8134 to be suitable for the job. I developed an evaluation board on the resources…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…