• ad8138

    AD8138可以驱动24位ADC嘛

  • AD8138 simulation issues

    Hello,

    I am trying to simulate a DAC interfacing with the AD8138 differential amplifier in LTSpice.

    The circuit is based on Figure 7 of MT-019

    The model used is the one available from the AD8138 product page and the simulation is the following:

  • AD8138 datasheet中的参数测试条件疑问

    1.单电源VS=5V时,差模失调电压定义为VOS,dm=Vout,dm/2;条件VDIN+=VDIN-=VOCM=0V是否应为2.5V?

    2.单电源VS=5V时,共模失调电压定义为VOS,cm=Vout,cm;条件VDIN+=VDIN-=VOCM=0V是否应为2.5V?

    3.单电源VS=5V时,VOCM共模抑制比测试条件ΔVOCM=2.5V±1V是否指的是VOCM=1.5V~3.5V?

    4.单电源VS=5V时,增益GAIN的测试条件ΔVOCM=2.5V±1V是否指的是VOCM…

  • AD8138: Diff-AMp Calculator issue

    I download the new version from website and have a try. Seems the value of Rf
    is double of the value it should be.
    For example, I designed buffer using AD8138, I set gain=1, Rg=200, Rf should be
    200, too, but it showed to be 422. Please refer to…

  • AD8138S and output protection diodes

    In our instrument we use AD8138S in configuration as depicted below. Unit A is separated from Unit B and the AD8138S are powered from separate power supplies VP_A, VN_A (unit A) and VP_B, VN_B (unit B). The analogue signal is transmitter over the harness…

  • AD8138S - SEE (Single Event Effect) Radiation Testing

    Dear Support,

    I'm looking for the SEE (Single Event Effects, like SEL, SEU, SET, etc.) values for AD8138S in MeV/mg/cm².

    Can you provide these parameters? TID vlaue in krad is not sufficient for analysing within our project.

    Thank you,

    Best…

  • AD8131 and AD8138 phase tracking info

    information regarding relative phase tracking for the AD8138 vs the AD8131

     

    The diff amps have a propagation delay, which adds a slight negative tilt to
    their open-loop phase responses.  To put this in perspective, one nanosecond is
    90 degrees…

  • AD8138 in wide band power amplifier: output balance error

    How do I get identical amplitude on each output node? We use test circuit for
    output balance (TPC 26).  We see balance error -40 dB (Vin 2V p-p, resistor
    tolerrance 1%).

     

    Please try measuring the output balance error , using the same…