• 关于AD8132仿真

    你好,在使用AD8132差分运放仿真时,有以一疑问,烦请解答
    1、输入一个0.2Vpp的交流信号,经过电阻以后,怎么只有0.083Vpp?

    2、Vocm脚在实际使用时可以悬空吗?

  • AD8132: Best way to drive baseband inputs, improve LO leakage

            1. The data sheet is specificity for a Vout = 2 Vp-p, I suppose that
    Vout=Vocm, then if I'll want to have 2 Vp-p at out, I'll must drive 2Vp-p at
    the Vocm input. But I don't know what is the value of -IN and +IN inputs.

  • AD8132 NC PIN

    Hi

    I hope you forgive me for a very trivial question.
    Does the NC (7) terminal of the AD8132 have an internal connection?
    This is a question just in case, so there is no problem at the moment.

    Best regards

  • AD8132 Bandwidth test problem(AD8132带宽测试问题)

    最近测试AD8132带宽,原理图完全按照手册推荐电路设计,PCB为双面板。大信号Vout=2Vp-p下,G=1,实际测试带宽只有254MHz,手册推荐值是350MHz;G=2,手册值是190MHz,实际测试136MHz。不知道是哪里除了问题,请有经验的大神帮忙分析下,谢谢!

  • AD8132 Use To Single Power Supply Input

    Dear All:

    AD8132 datasheet show "Power supply range: +2.7 V to ±5.5 V" If need to use single supply ,V– link to GND ,V+ can link +10V power source (0~10V) ??

    Best

    Jack

  • about headphone amplifier using ad8132

    Hi support,

    now I’m using ad1832 as an unbalanced to balanced headphone amplifier.

    although these usage is not recommended, I found this device reproduce

    hi-end quality sound. (great!) but I can’t reject EMI. when I move smartphone close to it…

  • RE: AD8132

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD8132 Vocm minimumum voltage.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9235 with AD8132(AD8138)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,