• RE: crosspoint-switch  AD8112  audio signal quality?

    Hi, Teodor.

    Sorry to keep you waiting.

    ADI has only two analog crosspoint applicable for audio and these are AD8112 (16X8) and AD8113 (16x16). With this, sorry to inform you that we don't have a 4x4 analog array.

    Regarding your THD question, both…

  • AD8112 - Is it possible to work with 3.3V Digital Supply?

    I need more information about the digital Supply Voltage of the AD8112.
    Which is the operating voltage of the digital part?
    Can I use a 3.3 volt digital power supply?
    If the the analog supply is +-5Volt and the digital supply is +5V, can…
  • AD8112 Vcc and Vee pins between pins 22-37

    What should I do with these Vcc and Vee pins? They are there for the output amplifier of the AD8113. Can I leave these disconnected when I'm using the AD8112? And where is the AVcc for output 7? It's not shown in the datasheet in figure 6.

  • AD8112_3: Are specs of the THD for the parts available at 1kHz? The datasheet only specifies THD at 20kHz

    Would it be possible to obtain the THD of the AD8112 and/or AD8113 at 1KHz?
    The datasheet only specifies this at 20KHZ.

     

    Here the answer from the Productline - the values are CALCULATED.

    The THD at 20 KHz and Vout = 20 Vp-p is 0.002…
  • AD8111_audio signal support

    One customer asked whether AD8111 can support audio signal? In AD8113
    datasheet, it specifies very clearly that it can support audio signal. The
    difference is that AD8113 can support +/-12V power supply if it is for audio
    signal switching…
  • TVI and CVBS MUX in the same chip

    I am trying to update a product in which we multiplex CVBS signals into a 1 of n selection.

    I would like to update the design to route TVI signals as well as CVBS signals.

    In our testing, we find that if all of the cameras are CVBS it works as it is…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225