Hi,
My customers want to make an integrator with AD 8099.
Is it OK to create an integrator with the AD8099?
<conditions>
Band: 10 to 10 MHz
Gain: 40 dB
Rf: 68 kΩ
Cf: 0.33 uF
Best regards,
Yuya
Hi,
My customers want to make an integrator with AD 8099.
Is it OK to create an integrator with the AD8099?
<conditions>
Band: 10 to 10 MHz
Gain: 40 dB
Rf: 68 kΩ
Cf: 0.33 uF
Best regards,
Yuya
Hi,
I use AD8099 as the output buffer of the AD768, for getting a ±1.1V output voltage. Specific circuit is in the attachment.
When I test this circuit, I found AD8099 is oscillating. Is there any suggestion to eliminate the oscillation of AD8099?
…Hello to everybody.
I am about to use the AD8099 in a low noise integrator. High bandwidth is really needed and 10 V supply too.
This is the best option I found.
Looking at the datasheet, I have troubles understanding the low voltage biasing scheme.
…Hi!
I purchased an evaluation board from Analog Devices for the AD8099 for inverting configuration and LFCSP package (product number: EVAL-ADOPAMP-1CP-1, user guide: UG-064)
I have problems soldering the LFCSP package. Can anybody give me advice?
…Hi there
I have attached a multisim simulation of a simple inverter amplifier using AD8099 (exatly according to AD8099 datasheet. Figure 60 Amplifier Configuration for SOIC Package, Gain = –1 ) which only works in simulation not in real world. Input…
Hi.
I am trying to simulate an AD8099 cascaded amplifier (please see the attached). Each stage amplifies x10, and the overall gain should be x100.
First I built the circuit using the FB pins of AD8099 as in the attached circuit and did an AC analysis…
Dear Supporter,
I have a query about AD8099. I use AD8099 in my product. The package is SOIC-8.
The power supply is +/-5V. The gain is set as -10.
Input signal is square wave with the frequency of 2MHz.
After increasing the input amplitude, the output…
Hi,
We have data for +/-5V and + 5V operating condition .
Do you have details of the Spec details when used at +12 V .
Thanking you
With best regards and wishes
Hi supporter,
I'm going to use an AD8015 to convert the current output from a photodiode,
following the AD8015 are two stage of AD8099 with both 5 times noninverting amplifying set (5x5 =25 times)
1.As the datasheet mentioned, the output impedance…