• Filter Wizard Design Equation(s)

    I am working on a 500 kHz active filter and turned to the filter wizard of Analog Devices. Given a center frequency of 500 kHz, 20 kHz passband, gain of 10 dB, it came up with a design using three AD8055 op-amp sections (attached below).

    Analog Devices…

  • RE: ADC前段,电压跟随器的选择

    您可以看一下ADA4817, AD8055, AD8057, AD8061以及AD8067这几个器件,压摆率满足您的要求,但请注意他们都不是轨到轨输入以及输出的放大器,要处理0~5V的信号的话,供电正轨要大于5V,负轨要低于0V,具体留多少裕量要参考具体的数据手册。

  • RE: Analog output interface for HS-DACs

    At lower frequencies, an op amp can be used to acheive differential-single ended conversion along with some gain if needed. For example, one recommended configuration for the AD9740 is shown below. Suggested op-amps for the interface are AD8055, AD8057…

  • AD9218

    Hi,

    I have some problems for designing a circuit based on AD9218. This is my first time to learn this IC, and make PCB layout by myself.


    The datasheet of AD9218 shows that pins 13,30,31,48 are the same pin for Analog Supply (Vd), but they aren't…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • RE: 超级干货——DAC接口基本原理

    DAC模拟输出考虑因素

    DAC的模拟输出可能是电压或电流。两者情况下,可能都需要知道输出阻抗。如果对电压 输出进行了缓冲,则输出阻抗将很低。而电流输出和未缓冲的电压输出将存在较高阻抗, 并还可能具有电抗性分量以及纯粹的电阻性分量。在有些DAC架构的输出结构中,输出阻 抗与DAC上的数字码字成函数关系,这点应会在数据手册中明确注明。

    理论上,电流输出应当连接到电阻为零欧姆的地电位。在实际应用中,该输出将采用非零 阻抗和电压。“顺从性”标题下只是定义了该输出可耐受的电压偏差大小,端接电流输出 DAC时应当注意到此项技术规格…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • 放大器输入保护...福兮祸兮?

    放大器输入保护是福是祸? 许多高速运算放大器都具有片上输入保护,在大多数情况下,这种保护对用户是透明的;但在某些应用中,这种保护可能是电路的致命弱点。来自ADI高速线性部门高级应用工程师John Ardizzoni在本文中为您分析输入保护的需求、实现及其潜在的缺点,并给出一些利用具有输入保护功能放大器的替代方案与电路方案。如果现在您还不能确定在您的设计中放大器输入到底是福是祸,那这篇文章一定不能错过哦!

    高速运算放大器的输入保护有多种形式,其中共模过压保护、静电放电 (ESD)保护、输入差分对保护是一些常见的保护…

  • ADI芯片辨识、型号查找

    看看截图: