• AD8051 & AD8091 absolutely identical, why two product codes?

    Studying data sheets for AD8051 & AD8091 I discovered that two ICs have no difference in theirs tech. specification, so question:

    why there are two product names / codes, or did I missed something ?

    https://www.analog.com/en/parametricsearch/11087#…

  • RE: AD725 and AD8051 thermal details

    Hi,

    Sorry for the delay. Here is the thermal data for AD8051.

    AD8051

    Theta-JC= 111.6 C/W

    Theta-JB= 68.46 C/W

    Best Regards,

    Jeyasudha.M

  • Alternatives to the AD829

    Alternatives to the AD829

     

    I can recommend alternatives though. Other single high speed opamps with
    Bandwidth > 120MHz and Slew rate > 230V/us are

    AD811 Single
    AD818 Single
    AD815 Dual
    AD828 Dual

    You will open up…
  • ADuC812: Status of the port on power-up

    - I use AD812 and wonder must I set the port 2 and 3 to  input/output n SFR or
    does it do that automaticly?

     

    Some information of the status of ports 0, 1, 2 and 3 on power up. Where the
    ADuC812 deviates from the "standard" 8051, I will explain…

  • RE: High speed AMP/ Video Splitter

    Any general purpose op amp should be able to meet your requirements.  Might look at the AD8051.

    http://www.analog.com/en/products/amplifiers/operational-amplifiers/rail-to-rail-amplifiers/ad8051.html#product-overview

    Within the data sheet there'e a reference…

  • RE: Bugs in spice models

    Hello Hooman,

    Thanks for your report.

    I have simulated with your examples.

    AD8061

    The input current in the simulation is +3.5uA. The datsheet also shows the same Ibias=+3.5uA.
    I also doubt that the sign of the bias current is correct. Every bipolar amplifier…

  • RE: ADL5513 log amp undershoot

    • You may be running into the ADL5513's own slew rate limitations; video BW will be dominated by the 3pF cap that is internal to the device on the CLPF pin
    • Have you just been looking at the output of the AD8051 buffer? Have you traced the undershoot…
  • Amplifier with low phase error DC-5Khz

    I'm developing a current sensing application that requires some amplification of the sensor output.

    One of the requirements is (ideally) zero phase error in the bandwidth of interest (DC-5Khz).  AD8051 looks to be unique among the AD parts I've examined…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • Need help selecting an op amp

    I am a digital designer, and a bit out of my element using op amps.

    I need to amplify a pulse stream using a single op amp stage [board already designed/fabbed around an SOT23-5 package]. I am currently using
    I need the highest gain I can get [10-20mv…