• RE: The BW of AD5452

    Hi Ivan,

    Thanks for your reply. The VREF I used is +-5.6 V, I think that is within the correct range.

    I just wanna design a signal generator by using AD9834,AD8030 and AD5452.The DDS component generates the signal ,use OPAMP  AD8030 to make it 18 - fold…

  • Constant current souce using LT8645S

    I've designed a constant current source based upon the LT8645S.  See attached. It works well when the load is around 1-2Ω.  But when I increase the load to 3-4 ohms, the current drops significantly.

    The input voltage is 42V, but the output voltage…

  • RE: powering AD8066

    Really your best bet is changing amplifiers to something like the AD8397 (less gain-bandwidth product) or AD8030 (closer) or even the AD8022 that at lease works at 4.5V. The AD8066 will probably work at 4.5 but you will have no guarantee of that. If this…

  • LTC7001 TS pin voltage issue when the INP signal is low

    Hi ADIExpert

    I have a BMS application usng LTC7001 as a high side switch as below schematic

    the issue is when I turn the U64/U65 off by asserting INP low (Vcc is still supplied with a 5V)

    I can still get a voltage (around )4.5V at V4_Pack+ node

    it looks…

  • LTC7001 application issue

    Hi ADIExpert

    I have a BMS application that use LTC7001 as the high side gate driver

    I would like to use 2pcs LTC7001 to form a back to back in order to be able to turn on-off each of the MOSFETs sets (Q145, Q146, Q147, Q165 set1 and Q151, Q152

    ,Q153,Q166…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADI芯片辨识、型号查找

    看看截图: