• Overview of AD8018

    I wonder which port is Input, Output, Vdd, Vss

  • Using for AD8397

    Dear Sir/Madam,

    I have a question.

    We are watching AD8018 datasheet page-1 FIg-2.

    If we replace the OPAMP from AD8018 to AD8397, then can we get the more high power current drive than AD8018?

    Thanks, Kaos

  • Questions for SSM2211

    Dear Sir/Madam,

    We have a question fo your SSM2211 audio amp.

    We will use your SSM2211 as RF amplifier for more power output instead of current AD8018.

    1)
    As for Page-12 Figure-35
    Thick Line=PHASE SHIFT
    Thin Line=GAIN
    Correct?

    2)
    As for same fig-35…

  • RE: a couple of question for AD8260

    Hi Kris,

    Thanks for your reply.

    I just confirmed your recommended 4-devices.

    AD8390

    The diff. output doesnt fit for our next stage.

    AD8397

    The peak AC current is smaller than AD8018 we are using at present.

    AD8016

    The output 400mA min - 600mA…

  • RE: High current drive op-amp?

    Two ways to go here - TI THS3091 with two in parallel, or paralleled AD8018 with a transformer to step up the output voltage.  Both are current feedback amplifiers, so pay special attention to the value of Rf in the data sheet.  If output phase is not an…

  • RE: What is the expected voltage range on the 2.5 V output on the ADALM1000?

    Hi:

    The original Bill of Materials for the production run of ALM1000 has the feedback resistor for the AD8018 buffer used for the fixed 2.5 V output at 24.9K which causes the output of the buffer to be lower than the desired 2.5 V by around 50 mV due…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…