• AD9889B,ADV7443,AD8017

    why can't I find datasheet of these devices from ADI website?

  • AD8017 single 5 V power supply operation

    AD8017 is configured for use on signle +5 V power supply. It is used for inverting(unity gain) the input signal. Rf = 619 ohms and Rg = 619 ohms. Rt = 52 ohms. The positive terminal(pin no 3) is connected to ground. 

    When an input signal (DC) voltage of…

  • AD8017 single 5 V power supply operation

    AD8017 is configured for use on signle +5 V power supply. It is used for inverting(unity gain) the input signal. Rf = 619 ohms and Rg = 619 ohms. Rt = 52 ohms. The positive terminal(pin no 3) is connected to ground.

    When an input signal (DC) voltage of…

  • AD8017 as op-amp follower over heat - current sinking

    Hello There,

    Having quite some trouble with the AD8017.

    The first stage is used as an amplification and the second one as a follower, it seem that the follower is sinking 200mA (seem to be limited by over-heat protection) current while the output is…

  • RE: ac constant current source

    Hi, siauhwa.

    AD8016 and AD8017 are amplifiers with high output current.

    Here are the links for their datasheets:

    AD8016 - http://www.analog.com/static/imported-files/data_sheets/AD8016.pdf

    AD8017 - http://www.analog.com/static/imported-files/data_sheets…

  • Detailed thermal models HMC8410 and others...

    Hi,

    I am looking for detailed or 2 wire resistor thermal models for the following devices: AD8017, AD9144, ADA4960, ADCL925, ADL5375, ADL5380, HMC7043, HMC7044, and HMC8410. I am working on preliminary thermal simulations and need more detail than the…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: Please recommend some buffers or drivers with high current driving capacity

    Hi Vic,

    Here is an Excel sheet with devices which have > 100mA output current sorted from high to low current for your review:

     XLSX

    Hope you can search through these and find a suitable part.

    Regards,

    Hooman

  • ADI运算放大器选型指南

    ADI运算放大器选型指南

  • ADI专家面对面之五——ADI产品介绍及其在各个领域中的应用

    ADI专家面对面是ADI公司与广大中小型客户以研讨会和客户拜访的形式直接交流的活动。ADI技术专家现场指导客户如何应对实际设计应用中面临的问题,并详细讲解了用户在实际应用中遇到的常见问题和解决方法。

    应广大客户的要求,我们将陆续上传ADI资深工程师们在研讨会现场的演讲PPT,以供大家参考,学习与探讨。

    目前更新至第五场研讨会的内容。

    第一场与第二场内容:深度了解168通道同步采样数据采集系统AD7606

    第三场内容:深入介绍放大器应用与经典案例分析

    第五场内容:ADI产品介绍及其在各…