• AD8016 PWDN pins

    Hello,

    I have an application in which I wish to use the AD8016 with +8/-5V rails at full bias current. 

    Do I need to drive the PWDN1:0 pins to a "TTL high" level to accomplish this, or can these pins float?  If I need to drive them, what is the…

  • driver board for amplifier AD8016

    Hi, we recently bought an evaluation board HSOPAMP 1RZ(8-Lead_LFCSP_Amplifer_UG-919) and amplifier AD8016. Then we found that AD8016 is 14-lead which is not compatible with this board. Could you please let me know whether there is an evaluation board for…

  • RE: AD8016 Digital and Analog Ground Pins/Packages...

    Hi Mike,

    Thank you for providing additional information. I tried simulating the differential amplifier configuration as in the Figure 41 of the AD8016 datasheet with the the same feedback and gain resistors as your customer. The simulation worked well…

  • Asymmetrical Suplies

    Can the AD8016 be used with asymmetrical supplies +18V/-5V?

     

    Yes. Anything within 26.4 total supply voltage is fine.

    Running the AD8016 from asymmetrical supplies is allowable, as long as the
    total supply does not exceed the absolute…
  • RE: 需要设计一个功率放大电路

    暂时没有相关的方案, 不过可以尝试一下AD8016/17, 其输出电流可以达到2A

  • RE: a couple of question for AD8260

    Hi Kaos,

    Apologies for the late reply. If you are only going to use the high current driver, you could check out AD8390, AD8397, AD8016 or AD8018 instead. Will these fit your application? Let me know if you have more questions.

    Thanks,

    Kris

  • RE: 运放选型求助(高速大信号)

    AD8016接近你的需求,你这个电压输出太大了,这种高电压的高速运放不好找。你可以多找几家芯片上,主要满足电压和带宽就行。

  • RE: Questions for SSM2211

    Hi, Kaos.

    DAC AD9762 has output current of up to 20mA only so why do you need a high output current amplifier of more than 400mA? Also, SSM2211 and AD8018 have almost the same output current of 350mA so better use AD8016 which has 600mA if you really…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…