• AD80066 clocks

    I'd like to use the AD80066 to digitise the outputs of 4 CCD channels whose maximum clock rate is 1MHz (each).  In many ways the part is perfect if it can run that slowly (ADCLK @ 4MHz).  The datasheet does not indicate any minimum frequency or maximum…

  • AD80066 clock

    I'd like to use the AD80066 to digitise the outputs of 4 CCD channels whose maximum clock rate is 1MHz (each).  In many ways the part is perfect if it can run that slowly (ADCLK @ 4MHz).  The datasheet does not indicate any minimum frequency or maximum…

  • Driving AD80066

    I'm using AD80066 to digitize four channels at 4MHz each (so ADCCLK is running at 16MHz).  I'm finding that the buffer amplifier I'm using to drive the ADC is oscillating.  I've tried AD8061, ADA4897-1 and AD8065; they all seem to oscillate…

  • AD80066 SHA mode

    Hello,

    I have a question about AD80066.

    My friend would like to use AD80066 in three channel SHA mode.

    I can see the timing chart of 1~4 channel CDS mode on P.6~7 of datasheet.

    But two and three channel SHA mode are not described on datasheet.

    Can…

  • Speed of AD80066

    Hello everybode,

    i want to use the "Complete 16 - Bit CCD/CIS Signal Processor AD80066" to convert the data from a CIS module.

    From the data sheet it's not clear to me, if the given frequencies are fix. I have different CIS modules in testing…

  • AD80066, outside data sheet !!

    AD80066, 

    Ive picked up a 'working' design, that 'just' needs some tweaks,

    Its an AD80066, running ALMOST as per fig 4 of the data sheet, 

        so its sha, but they are driving it as two channels , not two,

    i.e. there are 2 adc clocks per…

  • Error in AD80066 datasheet

    I'm not sure if this is the correct place to report this, but I can't find a more obvious place.

    I've been trying to use the AD80066 in 4-channel mode.  I got strange results for a long time (e.g. output value increasing as input voltage decreased…

  • AD80066 参考电路

    请问:AD80066与线阵CCD(TCD1304AP)的连接电路图在哪里可以找到?

  • AD80066 输出精度

    我使用AD80066做线扫相机的数据采集,实验发现其输出精度非常低,

    我的设置:使用4通道SHA模式,OFFSET引脚接地,配置寄存器设置为0x0F(此时能够测得CAPT − CAPB电压为1.5V左右),在输入通道接地的情况下,输出高字节的最低位都会出现1,希望能够提供帮助?!

    图纸如下:其中R20去掉,R19焊接0R,C39/C40焊接零欧电阻,C35/C36/C37/C38使用0R电阻