• AD8005 - Usage Vs at +3V at own responsibility

    Does the AD8005 can be operated at lower voltages, for example, +3 V?
    Which parameter changes are to be expected?

     

    We cannot guarantee anything about the AD8005 performance outside of its
    specified supply range from +5V to +/-5V. 
  • RE: symbols referenced in processor 'p0' could not be resolved: ADIAPI_OsdGetVideoFrameRate()

    Hi,

     In osd_control.c, you can get the definition of above api (ADIAPI_OsdGetVideoFrameRate).This osd_control.c file is not included in your project because in Visual DSP Project, 800X_BF_SW software folder is just empty. So you should paste the software…

  • RE: DDR memory interface of ADV8005's IBIS-model

    Hi,

    Please refer Page147,148 in AD8005 software manual,there we have registers for adjusting(read/write) the drive strength of DDR memory.

    Thanks,

    Poornima

  • RE: ADV8005 - Application Video Walls

    Hi,

     ADV8005 cannot support splitter mode i.e with one HDMI Rx input and two HDMI Tx outputs, But it can support PIP functionality.

     ADV7625 supports a splitter mode of operation, which enables the video content on one input path to be simultaneously routed…

  • [ADV8005] OSD fails to show on TV

    We port ADV8005_VSP_1.81RC1 to an MCU. To replace BF524 on EVAL-AD8005-SMZ board (printed on the silk screen: A0416-2013 REV 0.2, ADV8003 ADVANTIV VIDEO EVALUATION BOARD, the board is equiped with adv7625, adv7842, adv8005.),

    1. i2c, spi, and control…

  • RE: Noisy AD9951 output

    Thank you for the reply, I certainly appreciate it. I will get some waveform photos (old vs. new board) and when I borrow

    a spectrum analyzer next week I will photograph the plots and send them along. I am not using the comparator to

    square up the…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 放大器输入保护...福兮祸兮?

    放大器输入保护是福是祸? 许多高速运算放大器都具有片上输入保护,在大多数情况下,这种保护对用户是透明的;但在某些应用中,这种保护可能是电路的致命弱点。来自ADI高速线性部门高级应用工程师John Ardizzoni在本文中为您分析输入保护的需求、实现及其潜在的缺点,并给出一些利用具有输入保护功能放大器的替代方案与电路方案。如果现在您还不能确定在您的设计中放大器输入到底是福是祸,那这篇文章一定不能错过哦!

    高速运算放大器的输入保护有多种形式,其中共模过压保护、静电放电 (ESD)保护、输入差分对保护是一些常见的保护…

  • 转发ADI模拟技术训练营——放大器初步

    转发ADI模拟技术训练营——放大器初步 by zrk787

    转发ADI模拟技术训练营——放大器初步

    目录
    第一部分:放大器的分类简介
    第二部分:使用放大器的一般性规则
    第三部分:选择放大器入门
    第四部分:使用网络资源
    第五部分:数据记录和报告撰写
    第六部分:实验和注意事项

    8664.attachment.pdf