• IBIS model of AD8003

    Hello,

    My customer use AD8003 in their ATE syystem and  requests IBIS model of AD8003ACPZ-REEL7.

    Would you provide IBIS model of AD8003 ?

    They request IBIS model of AD8003 again even though they already confirm SPICE model in ADI web. site,

    Please provide…

  • RE: regardign IBIS model of AD8003

    Hi Mayuri,

    AD8003 is an analog part, so there is no IBIS model for this. We, however, provide its SPICE Model which can be downloaded here. AD8003 Product Page.

    Regards.

  • Question for AD8003ACP-EBZ

    Dear Sir/Madam,

    AD8003ACP-EBZ is only bare board that it show on your datasheet.

    So if we buy this, then can we get one AD8003 on there?

    Otherwise should we buy AD8003 for put on this?


    Thanks Kaos

  • orcad error of imported SPICE model AD8003

    Dear Sir/Madam,

    Our customer met one trouble.

    After import your SPICE model AD8003 to orcad PSPICE16.5, then the following parts have built .

         AD8003

         RVAR

         SWHYSTE3

    When he do his simulate to use AD8003, then the following error has comin.

         ERROR…

  • RE: AD8003 amplifier bandwidth under spice

    Hi Jino

    Thank you very much for the clarification.

    Is there any feedback resistor value that allows to change (reduce) significantly the bandwidth of the AD8003 when used in a gain=+1 circuit ?

    Thank you

    Best regards

    RB

    De : JinoL

    Envoyé : vendredi…

  • RE: DDS输出信号的功率放大

    您好!您可以看看AD8001和AD8003

  • RE: Inquiry about AD8003

    Hello Poornima,

    Thanks for responding, but I'm asking about the AD8003 (triple video CM

    opamp),

    not the ADV8003 (which is a whole different thing).

    Dana

    On Wed, Mar 21, 2018 at 8:47 AM, PoornimaSubramani <

  • RE: Ground plane under AD8003 and what to do with unused amplifier?

    Hi Joshua,

    Are you using the AD8003 evaluation board?

    In the connection diagram section of the AD8003 datasheet, it is recommended to connect the exposed pad of the part to GND or power planes or it can be left floating. Generally, the LFCSP is designed…

  • RE: Amplifier Selection?

    Hi Einstein,

    I suggest you add AD8000 (1.5 GHz Ultrahigh Speed Op Amp) and AD8003 (Triple, 1.5 GHz Op Amp) to your Op Amps consideration, both are current feedback amplifiers. Current Feedback amplifiers offer wide closed-loop bandwidth, low distortion…