• AD7992-0驱动代码问题紧急求救

    你好,最近在用AD7992,驱动是参考AD7991代码的,但是我看AD7991驱动的时候,有个delay(1000);这个代码延时大概是多长,我按照时序图写的代码不知道为什么一直读取出来的数据是FF,希望能得到官方支持。谢谢,希望尽快回复。

           AD7992_CON=0;

      Delay_us(10);

      AD7992_CON=1;

      Delay_us(10);

      AD7992_CON=0;

      Delay_us(10);

      IIC_Start();

      IIC_Send_Byte(0x21…

  • RE: AD5933 Clock Scaling

    thank you,

    i think same connectors are used on AD7991 eval board.

    i'm willing to buy AD5932 eval board and need to know the type of connectors on the AD5932 eval board, are they SMB connector?

    regards

    Nitin 

  • Interfacing with AD799x series ADCs

    Hi, all

    I wonder if anyone had success with the Digilent PMODAD2 ? The pmodAD2 has a ADI AD7991 ADC with a I2C interface. However the demo provided by Digilent can not work with Lx9Micro board. Any Suggestions ?

    BTW : can I config the I2C using the…

  • 2013年1~3月ADI征文大赛获奖名单公布

    20131~3ADI征文大赛获奖名单

     

     

    本期获得ADI征文大赛奖的网友和文章如下:

     

        ID

    标题

    名次

    xz19921230

    [征文]+[原创] AD9851应用心得(两片)

    1

    滔滔江水

    [征文]+[原创]TR组件中ADF4350调试经验分享

    1

    cpbe22

    [征文]+[原创]…

  • RE: ADC选择

    采样率大致可以有转换的时间来计算,也就是1/80us=12.5KHz,那么也就是ADC的采样率必须要大于12.5KSPS。推荐的型号请参考附件。

  • ADI中文技术论坛13年度精华帖盘点:转换器专区-专家解答热帖汇总

    AD9288 输入与输出的对应关系是什么??     

    http://ezchina.analog.com/message/9029#9029

    AD5934模拟IIC通讯的问题        

    http://ezchina.analog.com/message/9724#9724

    关于AD7763内部增益寄存器问题     

    http://ezchina.analog.com/message/9439#9439

    AD7606采样问题  

    http://ezchina.analog.com/message/8605…

  • RE: Measurement of pulse amplitude - suggestion for ADC

    Hi Henning,

         We have some I2C ADC interface that may fit your application, you may check the AD799x. Just like to ask on when are going to use the trigger feature, is it when the pulse amplitude hit some kind of limit or outside the range? I am also…

  • ADI芯片辨识、型号查找

    看看截图: