• AD7980... what do I do wrong?

    Hi,

    I simply want to connect an AD7980 to an Altera FPGA.

    The AD7980 is set in CS\ mode 3 wires with (or without, both methods tested) busy indicator.

    Everything looks perfect, except when the input voltage reaches some specific values corresponding…

  • AD7980的地?

    AD7980的地是模拟地和数字地的共用地。我的原理图设计上的模拟和数字磁珠隔离的,还有AD的调理电路。在连线的时候,能否将IN-作为模拟地,而GND作为数字地?

  • Add 2x daisy chained AD7980 instances [ AD7980 Project ]

    Having modified and flashed the Eclipse AD7980 Eval Board application in Bemicro NIOS II, I now need to add

    2 more AD7980 instances to Quartus II design in a daisy chained configuration.

    Can you share the steps necessary to 2x "instances" of the same…

  • AD7980的引脚GND等

    您好:

        AD7980的GND是数字地还是模拟地?AD7980的VDD是模拟电源?VIO是数字电源?不知道我的理解对不对。求解答。

  • AD7980的驱动

    您好:

    AD7980 - No-OS Driver for Renesas Microcontroller Platforms [Analog Devices Wiki]

       上面的网址是在ADI网站上查到的AD7980的驱动,我下载了看了一下,有几个疑问想请问一下。

       在“AD7980.c”这个文件中,有如下程序

    txData[0] = 0x7F;

      SPI_Write(0, txData, 1);

    上面的语句是不是作为延时用的?txData也可以不是0x7F?

    此外,AD798…

  • AD7980的IN-能不能接+2.5V

    工程师你好,我想AD转换一个双极性的单端信号,我打算将Vpp=5V双极性单端信号用差分输出放大器,转化为单极性差分信号,基准电压为2.5V,那么两个输出端子是不是都是在0到2.5V之间变化,那么选择AD7980的话能不能实现,也就是AD7980的IN-能不能接+2.5V,

    AD7980在选型表里显示是单极性差分信号输入,但是在技术文档里,写着是伪差分模拟输入。如果是单极性差分输入的话,IN+和IN-应该都是可以变的,但是IN-在技术文档里写着只能在-0.1到+0.1之间。

    能不能帮我介绍几款…

  • AD7980的时钟周期问题?

    您好:

        我现在使用的一个微处理器的SPI最大时钟18MHz,如果用一个AD7980工作在CS模式下,无法达到最大采样率1MHz,我根据时序计算得到的采样频率最大是600多kHz。

    我不知道我算的对不对。能否告知如何根据SPI最大时钟18MHz计算AD7980能工作的最大采样率的方法及最大采样率?

  • AD7980采样低电平采样值存在偏差问题

    设计中通过多路选择器+AD7980的方案来实现多通道数据采集,并在CNV上升沿时刻进行多路选择器切换,且相邻两个CNV之间为1.5μs左右,实测中发现当多路选择器在大电压范围切换时,比如0V和5V,会出现0V采样值为十六进制“07 XX”左右,与理论值相差甚远,与不切换时0V的采集结果也相差较大,请问这种现象是什么原因?在使用上通过什么方式可以规避?

  • Flash Programmer Problem [ AD7980 Project ]

    I can run the modified Eclipse APP for AD7980 using Run Configurations, and verify it using ucProbe. The Bemicro verifies the new code by lighting an extra LED. The Eclipse console says:

          Verified OK                 

          Starting processor at address 0x00010184

    I can…

  • ucProbe problem [ NIOS II AD7980 project ]

    Trying to recreate the NIOS II AD7980I project, I am running into a problem at the very last step

    with the uc-Probe:

        Clicked "Acquisition" button, ucProbe doesn't go through Acquisition, Transfer & Process states.

    1) NIOS II Eclipse…