how to buy ad7944 evaluation board and please clarify the usage of it
how to buy ad7944 evaluation board and please clarify the usage of it
Hi Forum,
is it possible to daisy-chain two different members of the AD794* ADC family?
I would like to use an AD7944 and an AD7942 and daisy-chain both devices to a single SPI bus, similar to Figure 36 in the AD7944 datasheet: AD7944.pdf
And if this…
Hi Usaghi,
There is an ADI that I also wanted to suggest the 14-bit AD7944 and AD7357
The AD7944 is pseudo differential analog input voltage range from 0V to Vref, Vref upto 5V while the AD7357 is a dual 14-bit differential ADC, which allows simultaneous…
Would it be possible to interface the BF592 to an SRAM via PPI to serve as a frame buffer. The system description consistes of: Analog sensor -> AD7944 A/D (2 MSPS @14 bit) -> processor via SPI. The goal is to capture 2 MBytes of data from the sensor…
Hi Rajesh,
I co-wrote the CN-0105, I'd like to make a few additional comments here. As for the ADA4899 vs.ADA4932, as Neil mentioned the ADA4932 provides better high frequency performance. The ADA4899 does offer better distortion performance at lower…
Hi Postino,
Here are some list of ADC that could be suitable for your application. You may also wanted to check the ADI website and do a parametric search and put in parameters on the ADC that you wanted to search. Please refer to the link below.
…Hi Henning,
We have some I2C ADC interface that may fit your application, you may check the AD799x. Just like to ask on when are going to use the trigger feature, is it when the pulse amplitude hit some kind of limit or outside the range? I am also…